Would like to evaluate the attached breadboarded circuit. The I/O on the PCA9539PW/Q900 would either be programmed to:
Can the float in #2 be achieved by enabling the I/O as an input?
Are there any recommendations on how to program an I2C sequence onto a breadboard?
Here's the updated file - thanks in advance for your feedback!
When an I/O is configured as an input, inside of FETs Q1 and Q2 are off, creating a
high-impedance input. The input voltage may be raised above VDD to a maximum of 5.5 V.
For IIC sequence and timing please refer to datasheet page10 -17.
thank you very much!