Configure Ds26521 T1 mode

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Configure Ds26521 T1 mode

Jump to solution
841 Views
shanmugamsundar
Contributor IV

hi all,

     I am using the ds26521 audio chip, in that i need to configure the T1 mode can any one help me with any basic settings on how to configure the T1 mode, is there any open source code is available, if so plz share the link

Thanks,

shan

Labels (1)
0 Kudos
Reply
1 Solution
590 Views
xiangjun_rong
NXP TechSupport
NXP TechSupport

The case is put in DSC group, can you tell me the processor you are using to interface with DS26521? the StarCore or DSC family, do you use DSP5685x family? I think you should interface Ds26251 with SSI rather than SPI.

View solution in original post

0 Kudos
Reply
1 Reply
591 Views
xiangjun_rong
NXP TechSupport
NXP TechSupport

The case is put in DSC group, can you tell me the processor you are using to interface with DS26521? the StarCore or DSC family, do you use DSP5685x family? I think you should interface Ds26251 with SSI rather than SPI.

0 Kudos
Reply