Can't TJA1145 do CAN Read/Write without SPI communication?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Can't TJA1145 do CAN Read/Write without SPI communication?

跳至解决方案
544 次查看
songinseok
Contributor I

Hi, 

I am going to do CAN communication using TJA1145 for this project.

I understood from the datasheet that TJA1145 enters STANDBY mode when powered on, and Tx/Rx does not work at this time.

At this time, I understood that in order to enter the mode where CAN communication is possible, the MC value must be set through SPI communication.


That said, CAN Tx/Rx via the TJA1145 seems impossible without SPI communication.

If possible, I would like to implement a circuit that enables CAN communication using TJA1145 without SPI communication.


Can't TJA1145 do CAN Read/Write without SPI communication?

 

Best regards,

Inseok

0 项奖励
回复
1 解答
532 次查看
TomasVaverka
NXP TechSupport
NXP TechSupport

Hi Inseok,

Your understanding is correct, the Normal mode can be selected from Standby or Sleep mode via an SPI command only, so the SPI communication is mandatory.

Best regards,

Tomas

在原帖中查看解决方案

1 回复
533 次查看
TomasVaverka
NXP TechSupport
NXP TechSupport

Hi Inseok,

Your understanding is correct, the Normal mode can be selected from Standby or Sleep mode via an SPI command only, so the SPI communication is mandatory.

Best regards,

Tomas