Hi,
I've found a file named<AN13117-Using the MC3377x to wake up the BMS master>, but it's for MC33771/MC33772, i wonder if MC33774 could wake up the BMS master, if it could, is there any file could introduce how to do?
Hi Long,
yes, the MC33775 and MC33774A are very similar. You can use the AN13117 also for the MC33774A, but please note, that some registers are doubled in the MC33774A since it is 18channels BCC and the registers are 16bits and following register addresses are moved accordingly.
With Best Regards,
Jozef