CLRC663: Power Amplifer Design

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

CLRC663: Power Amplifer Design

2,142件の閲覧回数
akashjain2996
Contributor II

Hi,

We are a designing a long range high power HF RFID reader based on ISO15693. To increase the range, we are planning a 4W system.

Is there any reference available for external power amplifier design?

How does the power amp affect the impedance matching? If so, what are the additional steps to be followed to during antenna matching circuit design?

2 返答(返信)

2,090件の閲覧回数
weidong_sun
NXP TechSupport
NXP TechSupport

Hello Akash,

    We have an application note on how to use external AMP for NFC reader, the AN is on document server.

    Customer can follow these steps to apply for the application note.

(1) Registerring an account on "https://www.docstore.nxp.com "

(2) logging in it.

(3) Searching "AN1425"

(4) below information will be found

pastedImage_2.png

(5) Downloading it.

Probably when you download it, you may be prompted "Waiting for administrator approval", then you can wait.

If not, you will be allowed to download it immediately.

Below is a block diagram of AN1425:

pastedImage_3.png

Have a nice day!

BR,

weidong

1,904件の閲覧回数
Guy_dor
Contributor I

Hello weidong

Will this work also on ISO15693 reader chip such as PN7462?

If so please help me to understand how.

Thank you

Guy

 

0 件の賞賛
返信