BGU8103 ENEBLE pin

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

BGU8103 ENEBLE pin

1,776件の閲覧回数
masahirokiniwa
Contributor IV

Hi,

Could you tell me about BGU8103 ENABLE pin?

If I apply Hi-Z to the ENABLE pin, is it pulled-down internally?

I would like to know the operating status, when it's applied Hi-Z.

(This situation will occur when I reset the controller IC.)

Best regards,

M.Kiniwa

0 件の賞賛
返信
4 返答(返信)

1,507件の閲覧回数
LPP
NXP Employee
NXP Employee

ENABLE pin is high input impedance signal. It doesn't have internal pull up/down.

Floating pin would cause unpredictable state between ON/OFF conditions.
Have a great day,
Pavel
NXP TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 件の賞賛
返信

1,507件の閲覧回数
masahirokiniwa
Contributor IV

Hi LPP‌,

Thank you for your answer.

Could you tell me an additional question about ENABLE pin?

Is it made of CMOS architecture or Bipolar architecture?

I care through-current when it is midpoint potential.

Best regards,

M.Kiniwa

0 件の賞賛
返信

1,507件の閲覧回数
LPP
NXP Employee
NXP Employee

I need some time to find information about input current requirements of this pin.

Please accept our apology for delay.
Have a great day,
Pavel
NXP TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 件の賞賛
返信

1,507件の閲覧回数
LPP
NXP Employee
NXP Employee

I've got a comment from the RF engineering team:

"

We strongly dont recommend the customer to leave the Enable pin float or HiZ. The status could be not stable. If the HiZ of GPIO is inevitable, they can connect a 100kOhm resistor from ENABLE to GND, which will force the LNA down once it is float.

BTW, during the reset process, please make sure the Venable<Vcc+0.6V, otherwise there is a risk to damage the LNA.

"

0 件の賞賛
返信