AN13725 - Where is the linker file?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

AN13725 - Where is the linker file?

454 Views
kowshik1729
Contributor II

Hi All,

I am trying to follow the AN13725 Appnote openCv cross compilation for RT1170 microcontrollers. My aim here is to follow similar process and compile openCV for a different microcontroller. I need the following info.

1. Where is the linker file mentioned in the opencv_mcu folder that's mentioned in the appnote?

2. What flags should be changed when using different armclang compilers (like ex: tiarmclang) because I am getting errors like CMAKE_CXX_Detection - Failed during the configuring stage.

3. Can we compile the source of the openCV without using the cmake setup? 

Thanks,
G Kowshik

0 Kudos
Reply
0 Replies