Dear All,
USBDM has been updated to V4.5. This is not a thoroughly tested version but is availble to provide support for the latest Codewarrior Eclipse version (10.1).
Please post any queries on this version in this thread,
bye
Notes
Please note that these design are different from the Freescale OSBDM-JM60 design which was proceeding independently while I was doing the above designs.
BDM History
Couldn't find correspoding topic for
USBDM/ Coldfire V2, V3 & V4 (combined TBLCF/DSC BDM) for JS16 and Codewarrior 7.2
The problem:
Works fine with CF Flasher and M5208EVB-like board.
Doesn't work with Codewarrior 7.2 programmer and hardware diagnostic.
All setup was done according with http://usbdm.sourceforge.net/USBDM_V4.5/USBDM_CF_JS16/html/index.html
I see led access activity on USBDM adapter and all signals at BDM connector observed with scope seems to be right.
WindowsXP SP3
Corresponding screen shorts attached.
Any Ideas?
Dear Kabron,
There is something strange with the second JPG posted. The dialogue is titled "MC56F800xx" which is the DSC interface. Are you using the correct GDI DLL as you appear to want to program a Coldfire chip?
bye
Hi pgo
The command line function is support for burning a single byte at the specified address on it? use RS08 or HCS08.
Thank you very much!
Dear pgo!
I try to use standalone programmer v4.5 to load code into board with MC9S12DP512 without success.
"Load Hex file" is withoout problem but after press "Programm" and some time I got " Programming Error - Programming of target flash failed! Reason: Flash command failed ( Bulk erase, Blank check or Program ) ".
In this time programming with Code Warrior ( HiWave ) is without problem.
I use hardware USBDM-JS16 with latest firmware and drivers.
We have idea what is the problem?
Thank you very much!
bendjy
Dear benjy,
I tried the JS16 BDM with a 9S12DP256B and a 9S12DT256 which are the nearest chips I have to the one you are using. I can't get any errors.
Do you get the error if you program a very small project that doesn't use paging etc. Is it specific to the project or does it happen with any project you create?
bye
Dear pgo!
Yes - the project is paged memory.
I will try to build other simple project and try to load in the board.
But board is very large with other controllers on it an many communication.
I will try to load it with small paged and small non paged project to check behaviour.
Thank You in advance!
bye
bendjy
Hi pgo,
I just checked the Gerber files for the USBDM JMxx and I'm missing the files
for the solder resist. Am I something missing or is this intentionally?
Many thanks in advance and best regards,
Robert