Hi,
Just a short question
I'm currently building my TBDML. I have tons of MAX232CPE chips and would like to use one of these to build my TBDML. I know the caps are not the same 1.0uF instead of 0.1uF caps (not sure) but also I think the CPE version is a bit slower.
someone is able to confirm that it should work with 1.0uf capacitor and a MAX232CPE chip ?
Thanks
解決済! 解決策の投稿を見る。
I used the file here http://forums.freescale.com/freescale/board/message?message.uid=5729#U5729
it use a max232 to put firmware into the TBDML mcu.
thanks
Hello,
Any type of MAX232 or similar would be suitable for this purpose.
Dear Lyncos,
I don't see how a MAX232 is useful for a TBDML. Do you mean a MON08 programmer?
I've used a MAX232CSE (which is similar) for this OK.
bye