I mean how to convert s19 file to ppt file?
Thanks!
cc.aa
HI
I answer your questions with red marks below. I admit my questions are not good enough, however, what I try to do is just to flash a S19 file into micro-p, and that's all. I didn't forecast that could be so terrible. Before this, I had no any experience of micro-P operations
Hi again,
Just let me establish what I am looking at here:
Please answer the following
1. You have built and programmed a TBDML?
I got a TBDML tool from China Tsinghua university, http://www.tsinghua-mot.net/kfgj/TBDML.htm
2. You have never used it before and so don't know if it works?
I never had the experience of it.
3. You have a fresh install of Codewarrior that you have never used to programme a MCU before?
Yes
4. You have a MCU on some kind of (homemade?) board that you have never programmed before?
Yes
5. So basically you don't know if anything works?
Yes
I am not trying to be smart here, just trying to narrow down the possible problem areas. At the moment there appears to be a thoasand possible issues.
Regards David
Ni Hao, (你好)
Ok, start from the begining.
When you plug in the TBDML does the computer make the ding, dong sound, like when you plug in USB peripherals?
Start CW then goto the hiwave debugger (or just run hiwave.exe from the prog directory. Then in the command window type "set gdi" without the quotes(").
Now one of the LED's on the TBDML should be flashing. On the status line at the bottom it should change from "No link to target" to "Target Ready". You don't need to connect the TBDML to anything to get this far.
I see in the picture that it has two leds. I assume one is power and one is the led i am talking about.
Let me know how you go.
Regards David (大伟)
Hi again,
Just let me establish what I am looking at here:
Please answer the following
1. You have built and programmed a TBDML?
2. You have never used it before and so don't know if it works?
3. You have a fresh install of Codewarrior that you have never used to programme a MCU before?
4. You have a MCU on some kind of (homemade?) board that you have never programmed before?
5. So basically you don't know if anything works?
I am not trying to be smart here, just trying to narrow down the possible problem areas. At the moment there appears to be a thoasand possible issues.
Regards David
Hi cc.aa,
1. Don't know. Can you select it as the target?
2. Yes, along with CodeWarrior!
3. Only by ensuring the s19 file is generated with the correct addresses within it. i.e. tell the programme that generates the S19 file where you want it to go.