Not able to flash hovergames os on navq

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Not able to flash hovergames os on navq

3,793件の閲覧回数
shardul
Contributor I

I tried flashing hower games linux image as per the docs both on emmc and sd card but failed.

here is the screenshot :

emmc

shardul_0-1632381315735.png

 

 

on sd card

shardul_0-1632381394353.png

 

 

 

 

Can someone help me with this as I am new to this.

Thanks

タグ(1)
0 件の賞賛
返信
2 返答(返信)

3,765件の閲覧回数
shardul
Contributor I

Thanks @Landon_Haugh , I am now able to flash os on SD card.

 But ran Into a different error.

I am not able to connect to navq using serial. With the old os on the sd card i have once connected to navq using putty. Then I disconnected all cables and tried again this time i was not able to connect to navq. I flash the latest os the one i mentioned before but still not able to connect to serial.

Would like to know if my board is booting properly. Attaching images of the board. 

 

shardul_0-1632443486487.png

 

 

0 件の賞賛
返信

3,775件の閲覧回数
Landon_Haugh
NXP Employee
NXP Employee

Hi Shardul,

 

The reason why your flash is failing on eMMC is probably because your NavQ has a 4GB eMMC chip, which was shipped out on most NavQ boards. Unfortunately, you can not flash the hovergames image to eMMC if you have a 4GB board, as the image is too large.

 

As for the SD card issue, can you try flashing the image before extracting the .bz2?

 

Thanks,

Landon

0 件の賞賛
返信