NXP FTF 2016 - トレーニングプレゼンテーション

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

NXP FTF 2016 - Training Presentations

ディスカッション

ソート順:
CARE enables hospitals and long-time care facilities to better measure, control and manage the overall patient satisfaction by combining a unique NFC-based patient skin-attached sticker and NFC enabled mobile devices with a care application and SMARTRAC's Internet of Things platform SMART COSMOS. The comprehensive solution provides a truly improved patient management, safety and comfort.
記事全体を表示
The course will detail RFC 7668 (6LoBLE), Bluetooth® low energy 4.2 and the Internet protocol support profile that are used to transport IPv6 frames in an IoT environment. The demo will be based on the Kinetis KW41 MCU.
記事全体を表示
Learn the basics of DDR4 and how to configure the DDR4 controller on QorIQ devices. Watch Video Presentation
記事全体を表示
Overview of the QorIQ LS2 and LS1088 processors, including the interfaces supported by the LS family, considerations while designing with these devices and use case examples. Watch Video Presentation
記事全体を表示
Ultra Wide Band (UWB) is just about to enter the automotive space. UWB in automotive NXP enables new convenience and functional safety use cases and an increased level of security. In this session we will discuss UWB - RF technology used in the automotive domain, specifically for secure car access systems. We provide an overview of customer needs and explain advanced features and the potential of this brand new NXP solution. Watch Video Presentation
記事全体を表示
This session will feature the LPC54114 MCU, the latest release of the LPC54000 low-power series, to demonstrate how to take advantage of dual-core architecture in always-on applications. Optimize product design for extended battery life and bring them to market quickly with this hands-on session. Topics will range from system architecture, software design and debugging, to power optimization, sound detection, and voice triggering.
記事全体を表示
Designing solid state RF solutions to deliver controllable, high efficiency energy for consumer cooking appliances requires designers to carefully consider size, cost, and performance objectives. This session will cover NXP's approach to a scalable, modular platform for delivering controllable RF energy for integration into cooking appliances. Watch Video Presentation
記事全体を表示
This session will provide a demonstration led by the instructor that showcases how you can develop end products using the application solution kit (ASK) for QorIQ LS1043A processors. Watch Video Presentation
記事全体を表示
Though cryptographic algorithms like AES are crypto-analytically secure, real implementations must at least be tested against logical attacks such as API misuse. Smart cards and similar devices also face fault and side channel attacks. Such attacks exploit physical effects to manipulate the device or learn about secret information. As these attacks are very critical, customers in the smart card industry ask for third party evaluation (e.g. Common Criteria or EMVCo) to confirm high assurance levels. If passed, a certificate is issued by a trusted party. With the rise of the IoT, physical attacks and respective third-party witnessing of resistance might soon be relevant there as well. Watch Video Presentation
記事全体を表示
Time-Sensitive Networking (TSN), a set of IEEE® 802 Ethernet sub-standards, is making deterministic Ethernet possible – especially for the automotive and industrial markets. This session will cover the advantages of TSN and current TSN standards and products. Watch Video Presentation
記事全体を表示
This paper will examine the use of an i.MX 6 IOT Gateway working together with a Cloud Services Platform (CSP), to collect and transmit data from a temperature sensor. The design options for seamless data transmission from device, to gateway, to cloud and then to a hand-held Smartphone will be considered and presented using Mentor Embedded Linux, Nucleus as well as Cloud Service Platforms.
記事全体を表示
With the very public hacks of some major vehicle brands in 2015, there is a renewed focus on vehicle security. There is a large range of vehicle electrical architectures, with significant regional variations, but there is an acceleration towards a domain orientated secure network. This presentation will look at the growing importance of the central gateway in a world of increased connectivity and security. As Ethernet becomes more prevalent, the topic of IP routing & firewall will be introduced and its role in adding another security layer. Finally, the role of the central gateway in enabling OTA software updated beyond the telematics unit, to the entire network will be presented.
記事全体を表示
Learn about NXP's newest technology for Single Chip System Modules (SCM) that provides ultimate customization and tiny form-factor via a unique vertical integration approach. Watch Video Presentation
記事全体を表示
This session will cover emerging trends in crypto acceleration APIs, their benefits, and NXP's roadmap for supporting them. Watch Video Presentation
記事全体を表示
The session will provide an overview of the most recent developments to support Radar systems in the frequency range from 76 GHz up to 81 GHz. High level block diagrams and key specifications of NXP multi-channel transceivers will be presented. It will also be discussed how the NXP transceiver solutions can help to enable modern low power consumption sensors with robustness against frequency interference, small size, and high-performance due to scalability. In combination with NXP Radar micro-processors and mircro-controllers typical Radar system architectures will be introduced. Especially for the development of small and compact cocoon, nano radar sensors an example is presented which shows the combinations of NXP Radar tranceivers, NXP Radar processors and NXP power supply solutions. The presentation will also give an outlook to technology trends and future upcoming NXP Radar solutions.
記事全体を表示
The LS1012A is the newest member of the QorIQ LS family, combining high-performance CPUs with line-rate packet processing. Learn more about this new class of product, including the many innovations made possible by its small form-factor and low power dissipation. Watch Video Presentation
記事全体を表示
Lecture on NFC commissioning and various use-cases NFC enables in Smart Home/IoT to save cost and enable convenience. NFC gives best of user experience for installing devices in Smart Home & Buildings and in-addition also useful for Diagnostic, de-commissioning, OTA upgrade and various other useful features.
記事全体を表示
ODP and DPDK are open-source project that defines a standard set of APIs for data-plane to be used across the different network processor architectures. This session details how the standard DPDK and ODP APIs are being mapped to NXP data-path acceleration for specific packet processing elements (packet IO, classification, scheduling, crypto, etc.). It also propose various possible API extensions to get additional performance on NXP SoCS. This presentation will cover how the ODP and DPDK can provide the necessary infrastructure for virtualized environments.
記事全体を表示
The RF content of connected devices has been increasing dramatically the last couple of years. The increasing bandwidth demand has driven the requirements of the RF chain to higher levels. The RF MMICs from NXP Smart Antenna Solutions give designers of connected devices freedom of antenna placement while achieving higher performance. This class will show the increasing requirements and complexity and NXPs answer to this challenge. Watch Video Presentation
記事全体を表示