Hello guys, i am working on a cover design project for PX4 robotic drone and i was wondering if anyone had a CAD file of the drone or the main body, that they could let me borrow?
Solved! Go to Solution.
Also the FMU Case is available here as well https://www.thingiverse.com/thing:3672194
okay thank you, and if you want to email me that cad file my email is guillermohuerta14@live.com
I did also post the STEP files (MCAD) on thingiverse here: https://community.nxp.com/external-link.jspa?url=https%3A%2F%2Fwww.thingiverse.com%2Fthing%3A4270674
when i opened the step file on solidworks it shows a circuit board, not the drone body? i dont know if im doing something wrong
ignore my last comment i figured it out. again thank you so much for the help man!
HoverGames Drone frame model by igalloway - Thingiverse
@Guillermo Huerta g_h89@txstate.edu Here is what i have found.
Dear @iaingalloway ,
When clicking the link provided above to the thingiverse page it is unable to download the detailed top-plate design which I require, all other parts are able to be downloaded and viewed/modified in Fusion 360. Is their anyway you could send me a direct copy of the detailed top plate as I require it for further development ?
Kind regards
Pards
I have this in MCAD. If you had time to help measure the details and write them down a bit i might be able to add more detail to the top and bottom plates ("frame-board")
I have added more accurate top plate file to thingiverse.
When reviewing the files in thingiverse It does not allow me to download the detailed top plate, even when downloading the entire folder whereby I am able to open/modify all the files in fusion 360, the only file that is missing is the detailed top plate as highlighted above. Is there anyway this could be rectified/sent directly to me ?
Kind regards
Pards
Hello, I am planning to build a mount for raspberry pi. Can I have the cad model of this or at least the dimensions of the plate? Thank You..
that'll work man, ill have to add the gps antenna since we have to work around that but i can do that. i appreciate it
Hello Guillermo,
The files will be available to download next week in the following link: https://www.nxp.com/design/designs/px4-robotic-drone-fmu-rddrone-fmuk66:RDDRONE-FMUK66
Thank you.
Hi Fabian, I think the files you are mentioning are the ECAD files (schematic and board files). Guillermo is looking for a mechanical design for the overall drone frame. I have an approximate one just about to hunt it down.
Meanwhile - there is a mechanical design for the FMU case here: HoverGames RDDRONE-FMUK66 RevC Case by igalloway - Thingiverse
were you able to hunt those files down Iain?
Just to clarify, this is for the physical drone, not the electronics or case for the flight controller (RDDRONE-FMUK66?)
I have a rough CAD file, but it doesn't quite give enough detail on the top plate where you would create a cover.
I'll check though various files and get back to you.
hovergames fmuk66 #rddrone-fmuk66
yes sir that's correct its for the physical drone, and i don't need too much detail. Thank you, i appreciate the help very much.