OM27462NBR: NFC-Bluetooth® Low Energy smart lock kit

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

OM27462NBR: NFC-Bluetooth® Low Energy smart lock kit

OM27462NBR: NFC-Bluetooth® Low Energy smart lock kit

Overview

OM27462NBR is a battery operated easy-to-use smart lock demonstrator kit for hospitality door access applications. The door operates by exchanging and verifying door access tokens via NFC and Bluetooth Low Energy. The design incorporates NXP® PN7462 first all-in-one full NFC Controller and the ultra-low-power Bluetooth Low Energy system-on-chip QN9021. The hardware is designed for low-power operation using a CR2 battery and features intelligent sleep and wake-up logic via Bluetooth Low Energy and a touch sensor using NXP capacitive touch sensor IC PCF8883.

The Bluetooth® word mark and logos are registered trademarks owned by Bluetooth SIG, Inc. and any use of such marks by NXP® Semiconductors is under license.

OM27462NBR Kit Content

OM27462NBR KIT content

OM27462NBR Full Kit Content

OM27462NBR Full Kit content

OM27462NBR Module

OM27462NBR Module

 

Specifications

Power ManagementBattery operated
Wireless
  • NFC and Bluetooth Low Energy design and operation
  • Token concept
    • Access token exchange and validation
    • ECDSA token signature verification
    • Smart card, Bluetooth Low Energy, and NFC via HCE token exchange
Support
  • MIFARE® DESFire® support
  • Android™ app available in Google Play™ Store
Ready to use

Documents and Software

User manual and Quick Start Guide are attached to this document

Labels (1)
Tags (1)
Attachments
Comments

Does anyone know if it is possible to configure this smart lock demo with a different nfc tag ie use a different nfc tag from the ones supplied with the kit?

Where can I find the software regarding this demo in case I need to reload the demo project after having loaded other software? ie how do you restore it to original software

 

Is there any source code for this demo?

No ratings
Version history
Last update:
‎05-08-2020 09:53 AM
Updated by: