how to change CLRC663 hardware to use SMA socket?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

how to change CLRC663 hardware to use SMA socket?

5,270 Views
m4416202
Contributor I


hello

         I have a problem that troubled me for a long time.I bought a piece of CLRC663 BLUEBOARD and a piece of LPC1769, and combine them to a NFC reader which can support most HF protocols.But this reader only can be used as "desktop reader".Now I want to change the hardware with the coaxial-cable(50Ω).So please help me or give me some methods.

thanks a lot

0 Kudos
Reply
5 Replies

4,498 Views
weidong_sun
NXP TechSupport
NXP TechSupport

Hi,

  please refer to attchment!

Regards,

Weidong

0 Kudos
Reply

4,498 Views
m4416202
Contributor I

孙工

能用中文沟通么?RC663有2个RX,而且是差分的信号,我现在按照方法2接的电路,其中RX2是悬空的,我想知道这会有多大影响?

方法2和方法3有什么区别,哪个接法性能更好?

NXP有类似CLRC663的UHF开发模块么,我一直没找到哎

谢谢

马阿龙

上扬无线射频科技扬州有限公司

扬州市广陵经济开发区创业路20号(科技创业园A3栋)

邮政编码:225000

电 话:18852574340

along.ma

Shang Yang RFID Technology Yangzhou Co., Ltd.

Building A3, No.20 Chuangye Road

0 Kudos
Reply

4,498 Views
weidong_sun
NXP TechSupport
NXP TechSupport

Hi 马工,

     2个RX来接收,就是为了增加接收信号质量的,具体的会造成什么影响,还要看你的应用环境是怎么样的,RF电路受环境影响是比较大的。

另外,其他的开发板,向PN532,PN5180,PN7120等有很多。

伟东

0 Kudos
Reply

4,498 Views
m4416202
Contributor I

孙工

我暂时就悬空吧,暂时没有发现其他的影响。

还有就是我指的是UHF超高频的开发板,不是高频的啊,因为NXP会提供全部的底层代码,所以我们也希望找到UHF的类似的开发板。

谢谢

马阿龙

上扬无线射频科技扬州有限公司

扬州市广陵经济开发区创业路20号(科技创业园A3栋)

邮政编码:225000

电 话:18852574340

along.ma

Shang Yang RFID Technology Yangzhou Co., Ltd.

Building A3, No.20 Chuangye Road

0 Kudos
Reply

4,498 Views
m4416202
Contributor I

孙工

     我就用中文问你啦,我现在是按照附件的方法2连接的,因为RC663有2个RX,所以,我现在的RX2是悬空的,不知道会有多大的影响?还有NXP有类似CLRC663的超高频开发板么?我现在也在找这个

谢谢

0 Kudos
Reply