Hi. I am using PN7150 in card emulation mode and was successful to transmit data from PN7150 to reader. But is it possible and if yes how can I write data from reader to PN7150?
Hi,
I am sorry, but are you using the NXP_NCI demo (https://www.nxp.com/webapp/Download?colCode=SW4325&appType=license&Parent_nodeId=1464843492338729907... ) or a custom application with PN7150? Please kindly clarify.
Have a great day,
Kan
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Yes, that demo just support read operation, but it is easy to add write support based on that demo, and if you need more details on that, please create a private ticket via the following link, and message me the ticket number.
http://nxpcommunity.force.com/community/CommunityContextPage
Thanks for your patience!
Have a great day,
Kan
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi Kan
You say easy, but I don't find it easy at all. I'm completely new to this NXP forum, but I have searched for quite some time now to find an explanation of how to modify SWA4325 so that I can write data to PN7150 in card emulation mode. I find it pretty impossible. Can you point me in a direction of how to do it, where to go to find some good documentation.
I see no reason to create a private ticket, as I think someone else than me might use the information later on.
Thanks in advance.
We have required a dll or explanation in this, no support useful is arrived. Thanks