Vdd and Gnd shorted NHS31xx

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Vdd and Gnd shorted NHS31xx

Jump to solution
1,704 Views
SnoZek
Contributor II

Hello,

I'm working on the NHS3152 demoboard and was working on the NHS3100 demoboard.

I'm working on it since few week and today i shorted Vdd and Gnd on processor but i can't figure why.

I listed few possibility :

 

-ESD (I have several per day with objects.

- Too much pin drive in same time (only 3 or 4 here) ?

- firmware (a problem in my code ?)

-Alimentation problem ( i use external alimentation) and diode still work

I had the same problem on my last demoboard. After days of operating it shorted.

if you have any idea i would be grateful.

 

Thank you for your time,

 

Yvan

Tags (1)
0 Kudos
Reply
1 Solution
1,699 Views
SnoZek
Contributor II

Update :

I tried to remove the component and put a new one. It work well now...

I deduce the cause of my problem was ESD. I should have taken more precaution about it before.

I put an NHS3100 on the NHS3152DEMOADK board. Could it be problematic ? Ofc i can't and use analog part.

 

View solution in original post

0 Kudos
Reply
2 Replies
1,700 Views
SnoZek
Contributor II

Update :

I tried to remove the component and put a new one. It work well now...

I deduce the cause of my problem was ESD. I should have taken more precaution about it before.

I put an NHS3100 on the NHS3152DEMOADK board. Could it be problematic ? Ofc i can't and use analog part.

 

0 Kudos
Reply
1,681 Views
driesmoors
NXP Employee
NXP Employee

Hi,

The IC's are pin compatible, so it should be OK. The same recommendations apply for both.

BR,
Dries.

0 Kudos
Reply