SLRC61003 Schematics design question

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

SLRC61003 Schematics design question

834 Views
bob_zhang
Contributor I

Customer is designing schematics using SLRC61003,there are two questions.

1 Their MCU power supply voltage is 2.5V,so they power VDD,PVDD and TVDD of SLRC61003 with 2.5V.I see the lower limit of these power is 2.5V in datasheet. Are there some potential risks for this design?

2 For TDO,TDI,TMS and TCK pins, If they don't use,how to deal with?Floating or Grounding?I find in demo design TDI,TMS and TCK are gounding  and TDO is floating.

I attach the schematic file,please help check.

0 Kudos
Reply
1 Reply

827 Views
weidong_sun
NXP TechSupport
NXP TechSupport

Hi Bob,

See below, please!

>>1 Their MCU power supply voltage is 2.5V,so they power VDD,PVDD and TVDD of SLRC61003 with 2.5V.I see the lower limit of these power is 2.5V in datasheet. Are there some potential risks for this design?

For SLRC61003HN, min voltage is no problem.

weidong_sun_0-1610446117561.png

In theory, there is no risk, but TVDD=2.5V, this voltage is relatively low, which will have an impact on the transmit power.

2 For TDO,TDI,TMS and TCK pins, If they don't use,how to deal with?Floating or Grounding?I find in demo design TDI,TMS and TCK are gounding and TDO is floating.

---You can design according to the method of DEMO board.

---In fact, there is no problem with these pins floating.

[Note]

  checked your schematic,  no other issues were found.

 Hope this information is helpful to you.

Have a nice day!

B.R,

Weidong

0 Kudos
Reply