Hi,
we bought the development kit PNEV7462B.
According to user manual UM10883.pdf we used following configuration
- chapter 3.1: External power supply
- chapter 3.2: VBUS set to 3.3V
Now we can't debug the device. We receive following message
15: Target error from Commit Flash write
When I set VBUS to 5V, it debugging is running.
According to manual, the device should run with 3.3V, or?
What else do I have to do?
Thanks and best regards
Stefan
Solved! Go to Solution.
Hello Stefan,
I checked schematic of PN7462AU EVK board and it's data sheet, in datasheet, there are some description on PVDD, see following,please!
-----------
8.15.2.2 PVDD_LDO
...
Hello Stefan,
I checked schematic of PN7462AU EVK board and it's data sheet, in datasheet, there are some description on PVDD, see following,please!
-----------
8.15.2.2 PVDD_LDO
...
Dear Weidong,
thank you for your anwer.
I closed JP42 and I replaced
- R179 to R177
- R181 to 180
it works, thank you very much.
Best Regards
Stefan