PN5180 ANT1 ANT2

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

PN5180 ANT1 ANT2

1,238 Views
yjshih
Contributor I

Hi:

   I just study the PN5180 development kit.  I cannot understanding these pins ANT1 ANT2 meaning and how to use them.  Do they mean if no power on PN5180, then PN5180 can act as card like Mifare card?

YJS 

0 Kudos
Reply
2 Replies

980 Views
AlanSbor
Contributor II


The antenna impedance tuning and measurement must be done with R = 10Ω between ANT1 and ANT2.

 

See AN11744   PN5180 Evaluation board

0 Kudos
Reply

1,037 Views
weidong_sun
NXP TechSupport
NXP TechSupport

Hello YJ,

   See following explainations,please!

(1) ANT1 & ANT2 are antenna connections when PN5180 is in PLM card simulation mode.

(2) In PLM card simulation mode, PN5180 is required to supply.


Have a great day,
TIC  Weidong Sun

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply