NFC Cockpit cannot detect board PNEV5190B

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

NFC Cockpit cannot detect board PNEV5190B

639 次查看
mbougouin
Contributor I

Hello,

I am trying to connect to my PNEV5190B Board, but NFC Cockpit doesn't seem to work.

The board is plugged on my laptop via an USB cable, and the board is powered up. When pressing the refresh button, software doesn't react.

NCF Cockpit's log seemed to indicate a problem with ADB process :

[2024.06.07 13:23:21]:DEBUG :ServiceBroker :MainWindow registration successfull
[2024.06.07 13:23:21]:DEBUG :ServiceBroker :ReadWriteNotify registration successfull
[2024.06.07 13:23:21]:WARN :OnlineVersionCheck :Please check your Internet connection!
[2024.06.07 13:23:23]:DEBUG :BoardDetect :Unable to load ADB process. Check if adb is part of environment variable
[2024.06.07 13:23:23]:DEBUG :BoardDetect :Exception details:
[2024.06.07 13:23:23]:DEBUG :BoardDetect : Type : System.ComponentModel.Win32Exception
[2024.06.07 13:23:23]:DEBUG :BoardDetect : Message: Le fichier spécifié est introuvable

VCOM files have been installed.

I changed USB cable.

0 项奖励
回复
3 回复数

620 次查看
KellyLi
NXP TechSupport
NXP TechSupport

Hello @mbougouin 

Please update NFC Cockpit fw, the attached for your reference.

0 项奖励
回复

572 次查看
mbougouin
Contributor I

Hello @KellyLi,

I am not sure that your answer is relevant.

It's NFC cockpit that's not detecting the connected board.

 

I can repeat my problem, with PNEV5190B board connected or not, the result is the same.

So I don't know why updating the board firmware will help me...

 

0 项奖励
回复

565 次查看
KellyLi
NXP TechSupport
NXP TechSupport

Hello @mbougouin 

What I mean is that you need to update the firmware of the board to NFC Cockpit as shown below, there is no VCOM port available from your log. Have you updated the bin file below?

KellyLi_0-1718014463587.png

 

0 项奖励
回复