Dear Support,
We have a project that needs to use MFRC522 as reader IC. We already have the experience with using NFC Reader Library v06.10.00, working with CLRC663 to host NXP/ST32L 32-bit ARM MCU and runs very well.
My question is:
I search relative topics below but not found the answer:
Best Regards,
David Huang
解決済! 解決策の投稿を見る。
Hello,
Yes, NFC Reader Library can't support for MFRC522. but I have some sample code for it, I will send it via email to you.
PS:MFRC522 is not recommended for new designs. For new designs, please use recommended product CLRC663 plus.
Have a nice day.
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-----------------------------------------------------------------------------
HI!
Could I get the sample code as well?
Thanks!
Hi,
Thanks for your prompt reply. I got the sample code you sent via Email.
I reviewed the sample code and knows it supports MIFARE Classic card. If possible, can you also provide the sample code for manipulating the MIFARE DESFire and MIFARE Ultralight card?
The reason why we use MFRC522 instead of CLRC663 is that the lead time of ARM MCU required by CLRC663 NFC Reader Library are 52 weeks or longer in Taiwan. Not like CLRC663, the MFRC522 can be implemented by 8-bit MCU, which has not the lead time issue.
Best Regards,
David Huang
Hello,
Yes, NFC Reader Library can't support for MFRC522. but I have some sample code for it, I will send it via email to you.
PS:MFRC522 is not recommended for new designs. For new designs, please use recommended product CLRC663 plus.
Have a nice day.
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-----------------------------------------------------------------------------
Could you please send me the example code on my email ?
Thank you
Hi fangfang,
Could you send me the example code to me, please?
Thank you very much.
Alex
Hi fangfang,
Could you send me the example code to me, please?
Thank you very much.
BR
Hugh Lin
Could you please share the sample code for the MFRC522?
Thank you!
Hi,
Thanks for your prompt reply. I got the sample code you sent via Email.
I reviewed the sample code and knows it supports MIFARE Classic card. If possible, can you also provide the sample code for manipulating the MIFARE DESFire and MIFARE Ultralight card?
The reason why we use MFRC522 instead of CLRC663 is that the lead time of ARM MCU required by CLRC663 NFC Reader Library are 52 weeks or longer in Taiwan. Not like CLRC663, the MFRC522 can be implemented by 8-bit MCU, which has not the lead time issue.
Best Regards,
David Huang
Hello,
Unfortunately, There's nothing else except the example code I sent you.
Have a nice day.
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-----------------------------------------------------------------------------