How to use Freedom KL25Z with Motor Shield L293D

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How to use Freedom KL25Z with Motor Shield L293D

Jump to solution
2,226 Views
rafaalvescomp11
Contributor II

Hi,

Is there a simple tutorial that shows how to configure the components and how to implement the motor control using the Motor Shield L293D with the Freedom KL25Z platform and the Kinetis Design Studio software?

0 Kudos
Reply
1 Solution
2,202 Views
nxf58904
NXP Employee
NXP Employee

Hi,

According to L293D's RM, you can set pins as gpio to determine the steering of the motor.

And you can set up a PWM to control the motor's speed.

 

View solution in original post

0 Kudos
Reply
3 Replies
2,202 Views
nxf58904
NXP Employee
NXP Employee

You should do is to configure pins as gpio and configure the pwm .

 

Have a great day,
TIC

 

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

 

0 Kudos
Reply
2,203 Views
nxf58904
NXP Employee
NXP Employee

Hi,

According to L293D's RM, you can set pins as gpio to determine the steering of the motor.

And you can set up a PWM to control the motor's speed.

 

0 Kudos
Reply
2,195 Views
rafaalvescomp11
Contributor II

Hi,

Thank you.

0 Kudos
Reply