MBD toolbox for S32K3 does not work in Linux

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MBD toolbox for S32K3 does not work in Linux

1,981件の閲覧回数
Nomados
Contributor I

I am using Ubuntu machine for the development

I successfully set up S32 design studio from NXP and was able to flash my

S32K3x4-Q257 board.

Also I was able to install the MBD toolbox, but it fails during the license check.

Since Linux does not have "vol" command I used my Ethernet address to generate license file.

However it always fails license check... I noticed that at NXP_MBDToolbox_S32K3xx/tools/mlt/ folder only has *.exe files that would not work in Linux.

 

Is there any way to use it with Linux? Toolchain seems to be compatible, only license activation is the problem!

0 件の賞賛
返信
2 返答(返信)

1,925件の閲覧回数
Nomados
Contributor I

Sorry to hear that... Do you have any plans to add support for Linux as well?

0 件の賞賛
返信

1,940件の閲覧回数
Irina_Costachescu
NXP Employee
NXP Employee

Hi @Nomados, 

The Model-Based Design Toolbox is a product developed and tested on Windows only, so, unfortunately, the Linux OS is not supported. For more details about the MBDT system requirements, you can consult the Model_Based_Design_Toolbox_S32K3xx_Series_Quick_Start_Guide document.

Regards,

Irina

0 件の賞賛
返信