Disconnected from "127.0.0.1" via 127.0.0.1.

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Disconnected from "127.0.0.1" via 127.0.0.1.

1,373件の閲覧回数
m15871781742
Contributor II

Hello:

      When i do the operating flash from file in the S32IDE according the "Model_Based_Design_Toolbox_MPC57xx_Series_Quick_Start_Guide"

      I have the following error :"MPC5744P Device detected.
                                                Interrupt command received. Halting execution.
                                                No breakpoints currently set.
                                                Disconnected from "127.0.0.1" via 127.0.0.1. Disconnection by port "55541" from 7224
                                                Target Disconnected."

      Does anyone know why?Thank you.

0 件の賞賛
返信
4 返答(返信)

681件の閲覧回数
rva3kor
Contributor I

Do we have a solution for this? 

0 件の賞賛
返信

1,193件の閲覧回数
Daniel_Popa
NXP Employee
NXP Employee

mikedoidge‌,

Any ideas on this ?

Thank you!

Daniel

0 件の賞賛
返信

1,193件の閲覧回数
m15871781742
Contributor II

sorry , i still haven't solved this problem.

0 件の賞賛
返信

1,153件の閲覧回数
MariusGavril
Contributor I

Hello,

 

Is this solved? Which is the solution?

Thank you!

0 件の賞賛
返信