Disconnected from "127.0.0.1" via 127.0.0.1.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Disconnected from "127.0.0.1" via 127.0.0.1.

1,434 Views
m15871781742
Contributor II

Hello:

      When i do the operating flash from file in the S32IDE according the "Model_Based_Design_Toolbox_MPC57xx_Series_Quick_Start_Guide"

      I have the following error :"MPC5744P Device detected.
                                                Interrupt command received. Halting execution.
                                                No breakpoints currently set.
                                                Disconnected from "127.0.0.1" via 127.0.0.1. Disconnection by port "55541" from 7224
                                                Target Disconnected."

      Does anyone know why?Thank you.

0 Kudos
Reply
4 Replies

742 Views
rva3kor
Contributor I

Do we have a solution for this? 

0 Kudos
Reply

1,254 Views
Daniel_Popa
NXP Employee
NXP Employee

mikedoidge‌,

Any ideas on this ?

Thank you!

Daniel

0 Kudos
Reply

1,254 Views
m15871781742
Contributor II

sorry , i still haven't solved this problem.

0 Kudos
Reply

1,214 Views
MariusGavril
Contributor I

Hello,

 

Is this solved? Which is the solution?

Thank you!

0 Kudos
Reply