Hi to all, using MQX SDK 1.0.0 (not beta) on KDS 1.1.1 with P.E. on FRDM-K64 The debugger stop me on a signal trap on:
Thread [1] <main> (Suspended : Signal : SIGTRAP:Trace/breakpoint trap)
__boot() at boot.S:66 0x7cc
the code where happen is:
/* Disable interrupts and clear pending flags */
ldr r0, =NVIC_ICER0
ldr r1, =NVIC_ICPR0
ldr r2, =0xFFFFFFFF
mov r3, #8
the line#66 is the ldr r0
what it mean this signal trap? what I can do to execute my code? (the code cycle for ever in this instruction)
thanks
Solved! Go to Solution.
Hi Massimiliano,
Please check the below thread an let me know if this helps!!
KDS and PE Micro Debugger Setup? | Freescale Community
Have a great day,
Sol
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi Massimiliano,
Please check the below thread an let me know if this helps!!
KDS and PE Micro Debugger Setup? | Freescale Community
Have a great day,
Sol
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Ok It seems that it was the problem
I workaround in another way
Hey Massimilano Sturla,
Could you please share your workaround?
Thanks,
Evgeny