UART doesn't receive data

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

UART doesn't receive data

ソリューションへジャンプ
4,639件の閲覧回数
albertolubeiro
Contributor III

Hi,

I am with a kinetis K64 with KDS 3.0 and KDSK1.2.0 and also with MQX.

My issue is that i do send data from UART to a PC terminal but i do not receive data from the PC terminal.

I am using the functions of "fsl_uart_hal.c"

This is my code after have initilized the UART

// Inform to start polling example

        byteCountBuff = sizeof(buffStart);

        UART_HAL_SendDataPolling(baseAddr, buffStart, byteCountBuff);

        // Inform user of what to do

        byteCountBuff = sizeof(bufferData1);

        UART_HAL_SendDataPolling(baseAddr, bufferData1, byteCountBuff);

    while (1){

        if (kStatus_UART_Success == UART_HAL_ReceiveDataPolling(baseAddr, rxChar, sizeof(rxChar)))

            {

                // Send any character that received

                UART_HAL_SendDataPolling(baseAddr, rxChar, sizeof(rxChar));

            }

    }

In the freedom, this code works fine in the example "uart_polling"

I understand that i have nothing to do with the interrupt since this is a waiting loop, isn't it?

the diference is that my project is based in MQX and the some files that i have had to change which are:

     -     pin_mux.c

     -     pin_mux.h

     -     gpio_pins.c

     -     gpio_pins.h

     -     board.c 

     -     board.h   

Any help will be apreciated.

Thanks and best regards

0 件の賞賛
返信
1 解決策
3,045件の閲覧回数
albertolubeiro
Contributor III

Hi,

i have solved the issue. At least i recive some data but still getting some issues trying to recive all data.

元の投稿で解決策を見る

0 件の賞賛
返信
4 返答(返信)
3,046件の閲覧回数
albertolubeiro
Contributor III

Hi,

i have solved the issue. At least i recive some data but still getting some issues trying to recive all data.

0 件の賞賛
返信
3,044件の閲覧回数
santiago_gonzal
NXP Employee
NXP Employee

Hello Alberto,

If you are using MQX, is the UART Polling the only task that MQX is managing? If not, what is the priority and the frequency of triggering of that task? And what is the baudrate?

Regards,

Santiago

0 件の賞賛
返信
3,044件の閲覧回数
albertolubeiro
Contributor III

Hi Santiago,

Yes, it is the only active task.

The priority is 10, it has an OSA_TimeDelay(100) and as for the baudrate i have checked it out with 115200 and 9600, with same result.

I try to send the word "alberto" and the buffer called "rxChar" may set to alberto, aertoal, lbertol etc...

and when this data must be send, all data are sent but 2. for example alber, aerto, lbert etc..

The code is below:

while (1){

        GPIO_DRV_ClearPinOutput(PTC18); //CTS

        GPIO_DRV_ClearPinOutput(PTC19); //RTS

        OSA_TimeDelay(100);

        memset(rxChar, 0, sizeof(rxChar));

        if (kStatus_UART_Success == UART_HAL_ReceiveDataPolling(baseAddr, rxChar, sizeof(rxChar)))

            {

                // Send any character that received

                GPIO_DRV_SetPinOutput(PTC18); //CTS     break point here so i can remove the RTS option in the PC terminal before send the data

                GPIO_DRV_SetPinOutput(PTC19); //RTS

                OSA_TimeDelay(100);

                UART_HAL_SendDataPolling(baseAddr, rxChar, sizeof(rxChar));

            }

    }

Thanks Santiago, and best regards.

0 件の賞賛
返信
3,044件の閲覧回数
santiago_gonzal
NXP Employee
NXP Employee

Hello Alberto,

Can you share the whole project? I want to see also the configuration parameters of the UART.

Regards,

Santiago

0 件の賞賛
返信