Hi
I have TWR-K20D72M and I read the quick start pdf of the TWR-K20D72M .I am Freescale MQX RTOS 4.0 BSP for TWR-K20D72M.
Now I want to read the ADC value which comes from the Potentiometer Already attach to the board. So I added ADC_LDD from processor expert and set the pin no. of the potentiometer mentioned in the Manual. My settings are shown in the picture attached. then I generate the code and build bsp.
My code for reading the value is below.
LDD_TDeviceData *Analog_DeviceData;
LDD_TError Analog;
LDD_TData *Buffer_DAta;
static uint16_t value;
void Analog_task
(
uint_32 initial_data
)
{
puts("\nInitializing Analog device.....");
Analog_DeviceData = AD1_Init(NULL);
if (Analog_DeviceData == NULL) {
puts("failed");
_task_block();
}
else {
puts("done");
}
for(;;) {
//AD1_StartLoopMeasurement();
AD1_StartLoopMeasurement(&Analog_DeviceData); /* do conversion and wait for the result */
AD1_GetMeasuredValues(&Analog_DeviceData,&Buffer_DAta); /* get the result into value variable */
printf("\n - Buffer_DAta = %d Hz", &Buffer_DAta);
puts(Buffer_DAta);
}
}
But no output Shown I change the value.
Can any one suggest me the efficient way of reading the ADC values using MQX and Processor Expert.
Hello Yogesh,
was this suggestion helpful? Please keep us posted :smileywink:
Best,
Monica.
Hi Yogesh,
I would suggest that you take a look to “CW for Microcontrollers v10 and MQX” which can be found at this path:
C:\Freescale\Freescale_MQX_4_0\doc\tools\cw
In page 64 you will find an explanation on how to add a new driver and specifically how to add ADC_LDD component.
I just ran a test using the pe_demo and added a task and it works with no issues. I am attaching the main.c file for your reference.
Hope this helps.
-Alí