Migrating from 60DN512ZVLL to 60DN512VLL

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Migrating from 60DN512ZVLL to 60DN512VLL

387件の閲覧回数
vines
Contributor III

Hi Geeks,

I am working on the older version 60DN512ZVLL for quite some time now. Everything is working fine. When we tried to migrate to the newer generation my ethernet is not working properly. I am using a custom board based on tower system. The new board is exactly the same as the old board except replacing the kinetis IC. I made the necessary changes on the BSP replacing the old chip with the new one. However, the new system's ethernet is not functioning properly. I can ping but TCP is not functioning properly. I am using the same application code.

On a side note, I loaded the telnet freescale sample program for the new chip (TWR60d100). However it is also not working. I find it odd because it is the sample program. Anyone who has a sample project and BSP for this new kinetis IC?

Do I need to explicitly set anything on the BSP (pull up or something) to make the ethernet for the new chip to work? I wonder if the phy chip that I am using is supported for the new kinetis chip  (KSZ8031)? 

FYI:

I am using MQX 4.0 and CW 10.4. I am using the ARM CW compiler not the GCC.

Thanks everyone.

0 件の賞賛
返信
0 返答(返信)