Hi,
I want to disable all IRQ on K64 for a short time. I found the following statement: "To disable all interrupts, use psp function cortex_int_disable in file cortex.c." But I cannot find a function cortex_int_disable(). Has anybody an idea?
Best Regards
解決済! 解決策の投稿を見る。
HI Andeas,
You can use the _int_enable() and _int_disable() functions, these functions enable and disable ALL interrupts EXCEPT NON MASKABLE interrupts becuase it is not possible to disable this type of interrupts.
These functions are defined in the mqx.h file, in addition you can find more information in Freescale MQX™RTOS Reference Manual(page 60), this manual is located at the path: C:\Freescale\Freescale_MQX_4_1\doc\mqx
Below you can find an example.
#include mqx_prv.h
#define WAIT_BLOCKED 0xF1
Restart(_task_id tid)
{
TD_STRUCT_PTR td_ptr = _task_get_td(tid);
_int_disable();
if ((td_ptr != NULL) && (td_ptr->STATE == WAIT_BLOCKED)){
_task_ready(td_ptr);
}
_int_enable();
}
Wait()
{
TD_STRUCT_PTR td_ptr = _task_get_td(_task_get_id());
_int_disable();
td_ptr->STATE = WAIT_BLOCKED;
_task_block();
_int_enable();
}
Have a great day,
Sol
Technical Support Engineer
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
HI Andeas,
You can use the _int_enable() and _int_disable() functions, these functions enable and disable ALL interrupts EXCEPT NON MASKABLE interrupts becuase it is not possible to disable this type of interrupts.
These functions are defined in the mqx.h file, in addition you can find more information in Freescale MQX™RTOS Reference Manual(page 60), this manual is located at the path: C:\Freescale\Freescale_MQX_4_1\doc\mqx
Below you can find an example.
#include mqx_prv.h
#define WAIT_BLOCKED 0xF1
Restart(_task_id tid)
{
TD_STRUCT_PTR td_ptr = _task_get_td(tid);
_int_disable();
if ((td_ptr != NULL) && (td_ptr->STATE == WAIT_BLOCKED)){
_task_ready(td_ptr);
}
_int_enable();
}
Wait()
{
TD_STRUCT_PTR td_ptr = _task_get_td(_task_get_id());
_int_disable();
td_ptr->STATE = WAIT_BLOCKED;
_task_block();
_int_enable();
}
Have a great day,
Sol
Technical Support Engineer
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------