MK60DN512 vs MK60DN512Z MQX issue

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MK60DN512 vs MK60DN512Z MQX issue

ソリューションへジャンプ
765件の閲覧回数
aroste
Contributor IV

Hi,

(CW10.5, MQX4.0.2)

I cloned the BSP TWR-K60N512 for my project that use a MK60DN512VLQ10.

In the BSP tower project it is a MK60DN512Z (define PSP_CPU_MK60DN512Z). I tried to change in PE the processor type (add new and disable the Z) and I have some issues in MQX files. (I2S mainly)

Can someone help me to understand why a uC that should not be used for new design (the Z) is supported in MQX and not the current one?  

Or maybe I am missing something but at this point I loose my minds.  (I checked the reference manual and I can see the difference in the IO_Map.h correspond to the differences in the manual)

I will try now the clone a BSP from the twr-k60d100m now to see the difference.

Thanks

BR

stéphan

タグ(2)
0 件の賞賛
返信
1 解決策
481件の閲覧回数
aroste
Contributor IV

At this point I succeeded by starting from the TWR-K60D100M that is the correct family.  I can see that the BSP files and all io files are related to the non-"Z" version now.    :-)

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
482件の閲覧回数
aroste
Contributor IV

At this point I succeeded by starting from the TWR-K60D100M that is the correct family.  I can see that the BSP files and all io files are related to the non-"Z" version now.    :-)

0 件の賞賛
返信