Is there a MQX 3.7 for CW 7.1?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Is there a MQX 3.7 for CW 7.1?

Jump to solution
679 Views
SVC2
Contributor II

It seems like MQX 3.7 supports only CW7.2

 

1)      The projects (mcp) files are not compatible.

2)      Even if I arrange the mcp files, I don’t think the code will compile since 7.2 is not backward compatible with 7.1

 

Is there a 7.1 version available?

 

Thanks,

S

0 Kudos
Reply
1 Solution
569 Views
petr_uhlir
NXP Employee
NXP Employee

Is there a 7.1 version available?

No, the support for older CodeWarrior for ColdFire 7.1 was removed in MQX 3.6.0

 

It seems like MQX 3.7 supports only CW7.2

 

1)      The projects (mcp) files are not compatible.

Only backward compatibility is maintained. The projects are converted to new version

 

2)      Even if I arrange the mcp files, I don’t think the code will compile since 7.2 is not backward compatible with 7.1

Hard to say, we have not generated and tested 7.1 projects.

 

Do you have any problems to switch to CW7.2?

 

 

View solution in original post

0 Kudos
Reply
2 Replies
570 Views
petr_uhlir
NXP Employee
NXP Employee

Is there a 7.1 version available?

No, the support for older CodeWarrior for ColdFire 7.1 was removed in MQX 3.6.0

 

It seems like MQX 3.7 supports only CW7.2

 

1)      The projects (mcp) files are not compatible.

Only backward compatibility is maintained. The projects are converted to new version

 

2)      Even if I arrange the mcp files, I don’t think the code will compile since 7.2 is not backward compatible with 7.1

Hard to say, we have not generated and tested 7.1 projects.

 

Do you have any problems to switch to CW7.2?

 

 

0 Kudos
Reply
569 Views
CarlFST60L
Senior Contributor II

I have just been forced to update to CW10.1 over the last couple of days due to lack of support for 7.2. Mostly for the D4D demo's.

0 Kudos
Reply