Hi I am using CodeWarrior 10.5 and MQX 4.1. I want to use DAC given in K70. Can anyone help me in locating the example code? or provide some example code for the same.

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Hi I am using CodeWarrior 10.5 and MQX 4.1. I want to use DAC given in K70. Can anyone help me in locating the example code? or provide some example code for the same.

ソリューションへジャンプ
648件の閲覧回数
sudhanshumehta
Contributor IV

Hi I am using CodeWarrior 10.5 and MQX 4.1. I want to use DAC given in K70. Can anyone help me in locating the example code? or provide some example code for the same.

0 件の賞賛
返信
1 解決策
520件の閲覧回数
danielchen
NXP TechSupport
NXP TechSupport

Hi

Currently there is no DAC driver for MQX.

You need to either use the Processor expert DAC driver or adapt the DAC 12-bit demo driver provided with CodeWarrior for MCU 10.5, Such demo is in the next path:

C:\Freescale\CW MCU v10.5\MCU\CodeWarrior_Examples\Kinetis_Examples\k60\dac12bit_demo

Have a nice day,

Daniel

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
521件の閲覧回数
danielchen
NXP TechSupport
NXP TechSupport

Hi

Currently there is no DAC driver for MQX.

You need to either use the Processor expert DAC driver or adapt the DAC 12-bit demo driver provided with CodeWarrior for MCU 10.5, Such demo is in the next path:

C:\Freescale\CW MCU v10.5\MCU\CodeWarrior_Examples\Kinetis_Examples\k60\dac12bit_demo

Have a nice day,

Daniel

0 件の賞賛
返信
520件の閲覧回数
sudhanshumehta
Contributor IV

Hello Daniel ,

I thank you for the reply.

I was familiar with processor expert. so i used that. it is really st. forward.

it is working..

thanks

Sudhanshu

0 件の賞賛
返信