Hello,
I want use BSP cloning wizard to create my own Specific target OS.
I followed instruction given in this post:
But on step 3, on the field "Board base" I have not choice, the list is empty. Then I can't continue...
Is anybody has an idea?
Solved! Go to Solution.
Hello,
I'm using Windows 10.
MQX 4.2 is installed in the default folder (c:\Freescale\Freescale_MQX_4_2)
I have just found how resolve this problem.
In Settings/Preferences, I clicked on "Restore defaults" button.
This make no change in the windows because my folders was already the default folder.
But after do "Apply" then "Ok", the list in "Board base" filed appears filled now!
...
Hi Arnaud:
What host operating system you are using? Windows 7, 8 or 10?
In addition, I suggest install MQX in the default folder.
Regards
Daniel
Hello,
I'm using Windows 10.
MQX 4.2 is installed in the default folder (c:\Freescale\Freescale_MQX_4_2)
I have just found how resolve this problem.
In Settings/Preferences, I clicked on "Restore defaults" button.
This make no change in the windows because my folders was already the default folder.
But after do "Apply" then "Ok", the list in "Board base" filed appears filled now!
...
Hi danielchen
I have am using windows 10, KDSV3 and MQX4.2 for TWR64 board. I am not able to run BSP Cloning Whizard. I see this error:
Based on the readme file(location: C:\Freescale\Freescale_MQX_4_2\tools\BSPCloningWizard\readme), I have installed latest JRE(jre-8u144-windows-x64.exe) and updated it. Am I missing something?
I had tried to run the BSP cloning wizard patch(FSLMQXOS_4_1_1_GA_UPDATE_BSPCW_1_5_GA.exe) but it seems to be looking for MQX V4.1 and as i am on MQX4.2, it didnt execute. Here's a screenshot:
Am I missing something?
Thanks in anticipation.
Best regards
Sarma