Hi,
I'm trying to porting my project under MQX 4.2 to fix a bug with MFS (MFS - file access error) and several other with RTCS.
The Wifi part seems to be completly changed without any explanations :smileyconfused:
- Some declarations are added for the Wifi in the BSP (init_enet.c) but nothing about where to place the Atheros files
- Includes for other modules are added and make errors because code source are not present (GainSpan, RedPine)
Is there a very new document about WiFi implementation ?
EDIT 07/24/2015 :
I put all the new lines in comments (init_enet.c and twrk60d100m.h) and re-use old code for Wifi.
There is a new problem in iwcfg.c, in the iwcfg_set_essid function :
uint32_t iwcfg_set_essid
(
uint32_t dev_num,
char *essid
)
{
_rtcs_if_handle ihandle;
ENET_ESSID inout_param;
uint32_t error;
bool dev_status;
if (dev_num < IPCFG_DEVICE_COUNT)
{
ihandle = ipcfg_get_ihandle(dev_num);
if (ihandle == NULL)
{
printf("Initialize Wifi Device Using ipconfig\n");
return ENET_ERROR;
}
if (!essid)
inout_param.flags = 0;
else
inout_param.flags = 1;
inout_param.essid = essid;
inout_param.length = strlen(essid);
error = ENET_mediactl (((IP_IF_PTR)ihandle)->HANDLE,ENET_MEDIACTL_IS_INITIALIZED,&dev_status);
if (ENET_OK != error)
{
return error;
}
if (dev_status == FALSE)
{
return ENET_ERROR;
}
error = ENET_mediactl (((IP_IF_PTR)ihandle)->HANDLE,ENET_SET_MEDIACTL_ESSID,&inout_param);
if (ENET_OK != error)
{
return error;
}
return ENET_OK;
}
printf("IWCONFIG_ERROR: Invalid Device number\n");
return ENETERR_INVALID_DEVICE;
}
After calling ENET_mediactl for the first call, the inout_param struct is crushed and the ssid string is corrupted. It needs to be reaffected (or only affected AFTER the first call) before call the ENET_SET_MEDIACTL_ESSID.
Yvan
解決済! 解決策の投稿を見る。
Solved : between CW10.5 and 10.6, I need to change the bool type (_Bool) by uint32_t.
Hello Yvan,
Thank you for sharing your solution.
Regards
Sol
Hi Sol,
This is just a workaround, not a solution. Solution to the situation, when there is obviously a never-compiled code in the MQX release, would be a prompt patch by Freescale.
I tried to fix the problem by adding the Atheros code in MQX and managed to build it successfully. I ran the httpsrv demo, but it did not work correctly. That's where I stopped, it is not my task to debug untested MQX features.
Can you please provide some official patch or initiate its implementation?
Regards,
Petr
Petr,
After several days and nigths, it's re-working for me. If you have specific question, ask me !
I think a AR4100 patch must be released by FREESCALE quickly (it's not the Qualcomm job since the last patch).
Yvan
Hi Yvan,
Thank you for your reply. It would be good to share some knowledge. Can you please follow me so I can send you private messages? Thank you.
Petr
Done !
Hmm, are you sure? :-) I can't see you in the followers list, nor I can send you a direct message...