set MPC5748G LINFlexD0 in Identifier mask mode

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

set MPC5748G LINFlexD0 in Identifier mask mode

560 Views
haiyang
Contributor III

board:DEVKIT-MPC5748G

IDE:S32DS PA 2.1

 

now ,i use the MPC5748G LIN0 interface ,i need to receive all message in the bus ;

so i nned set it to Identifier mask mode ,if there has some demo code?

the "MPC5748G-LINFlex-LIN-Master-Slave-test-GHS616" code is in Identifier list mode , not fit me

can you help me? 

 

0 Kudos
Reply
5 Replies

553 Views
PetrS
NXP TechSupport
NXP TechSupport

Hi,

you should be able to modify a code for your need. Check chapter 45.4.2.6 Identifier filtering of the device RM and change IFER, IFMR, and IFCRn accordingly.

BR, Petr

0 Kudos
Reply

528 Views
haiyang
Contributor III

HI,

i use Lin0 in slave mode and i set filter as follow:

LINFlexD_0->IFER = 0x03;//
LINFlexD_0->IFMR = 0x01;//
 
 
LINFlexD_0->IFCR[0] = 0x15;//
LINFlexD_0->IFCR[0] |= 0x07<<LINFlexD_IFCR_DFL_SHIFT;
if (g_Lin0Cfg.checksumMode==CLASSIC_MODE)
{
  LINFlexD_0->IFCR[0] |= LINFlexD_IFCR_CCS(1); 
}
 
the Lin0 can receive all id , but it only can receive the message which lenth = 7 ;
i want receive all lenth message , how to config?
 
0 Kudos
Reply

515 Views
PetrS
NXP TechSupport
NXP TechSupport

Hi,

this is proper behavior. It is described in the RM
Screenshot 2024-05-23 134557.png

if there is match with filter then DFL, CCS, DIR is given by value set in IFCR. 
In case of no filter match and BF is set then you get RXI interrupt upon header reception and you can specify BIDR.

BR, Petr

0 Kudos
Reply

512 Views
haiyang
Contributor III

thank  reply

but ,when get into RXI ,i still  don't know how many bytes data will come in,may be 1 byte ,maybe 2 ,maybe 6...

so when into RXI ,what should write to BIDR?

0 Kudos
Reply

510 Views
PetrS
NXP TechSupport
NXP TechSupport

Hi,

on LIN systems this must be know in advance, during system specification, thus the ID specify payload, direction, CCS.
You cannot receive unknown payload using LINflexD.

BR, Petr

0 Kudos
Reply