USB module reset bit is always 1, what may be the problem?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

USB module reset bit is always 1, what may be the problem?

118 Views
H-chips
Contributor I

In using MPC5748G as main control chip to try to write the development of USB device, using the SDK after introducing the USB module, the path to the SDK/middleware/USB/device/" of the function.

 

After executing USB_DeviceInit, the program stops here:

sdk.png

 

reg.png

 

 

MPC5748G-GW-RDB 

0 Kudos
Reply
2 Replies

104 Views
davidtosenovjan
NXP TechSupport
NXP TechSupport

Pay attention to following thread:

https://community.nxp.com/t5/MPC5xxx/MPC5748G-USB-Command-Reset-Issue/m-p/731260

I believe it could be possibly the same issue.

0 Kudos
Reply

91 Views
H-chips
Contributor I
Thank you for your answer. I have read this post, it should not be the same problem, it does not give the exact solution, but according to the description of the reply, I feel that it may not be the same problem, temporarily found a possibility, perhaps the hardware circuit problem, whether the CPEN of USB3340 must be connected with a power switch? I'm just pulling up the VBUS
0 Kudos
Reply