I just bought a second (I'm a big spender) TRK-USB-MPC5643L, and when it arrived the bag was marked "REV B".
Comparing with my Rev A, the only obvious difference, besides the silkscreen, is the addition of J11, which (no surprise here) doesn't appear in my Rev A schematic.
Does anyone know what J11 does? It comes not-connected (no jumper installed, e.g.); should I just leave it that way?
More generally: Are the Rev B schematics available somewhere?
已解决! 转到解答。
Hi, I have just obtained Rev B schematic (see attachment). J11 only enables pull-up for CAN0_RXD pin.
On the bottom of the board there is a (silkscreen) box with two lines: "SCH-27701 / 700-27701" . This marking is the same for both boards.
On the top of the board there are 3 lines: "SPF-27701 / TRK-USB-MPC5643L / "<copyright>, where <copyright> is "(c)2012 FREESCALE" for the old board and "(c)2016 NXP" for the new one.