SPC5746C core HVD_LV_cold monitor problem

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

SPC5746C core HVD_LV_cold monitor problem

645件の閲覧回数
kangjia123
Contributor I

Hi expert,

I have active the over voltage detector HVD_LV_cold by the configuration as below, but the test result fail to meet the requirement. The MCU fail to reset when the MCU core voltage is overvoltage.

besides, I want to confirm that  the specific  manifestation for functional reset  is MCU reset, right?

1. MC_RGM_FERD: Bit14 and Bit17 are set to 0.

kangjia123_0-1637129983188.jpeg

kangjia123_1-1637129983216.jpeg

2. PMCDIG_MCR: bit 20 and bit21 are set to 1.

kangjia123_2-1637129983252.jpeg

 

タグ(1)
0 件の賞賛
返信
1 返信

626件の閲覧回数
PetrS
NXP TechSupport
NXP TechSupport

Hi,

HVD feature can be enabled/disabled using UTEST_MISC[HVD_EN]. By default it is disabled.

BR, Petr

0 件の賞賛
返信