S32R294 RSDK CTE register write fault

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S32R294 RSDK CTE register write fault

1,344 Views
zhuyuechong1
Contributor I

Hi all:

In the S32R294 RSDK demo, when we write the CTE register ,there must be a fault.

Fitst we config the CTE0_CLK to 80MHz.

{.clockName = CTE0_CLK,

.mc_me_RunPeriphConfig = MC_ME_PERIPH_CONFIG_1,

.mc_me_LowPowerPeriphConfig = MC_ME_PERIPH_CONFIG_0}

after that , we config the CTE register such as "CTE.CNTRL.B.MA_SL_ST..=.1;"

there will be a fault 

"No source available for “0x0”",

So  how can we config the CTE register?

0 Kudos
Reply
4 Replies

1,199 Views
georgebogdandum
NXP Employee
NXP Employee

Hi,

please give me more information about the software version you use, it seems there is a mismatch somewhere.

0 Kudos
Reply

1,262 Views
georgebogdandum
NXP Employee
NXP Employee

Hi,

it seems the CTE clock is not really on.

Please check the entire setup to see if the clock is correctly activated. It is possible to check the clock frequency using CMU_FC_2.

0 Kudos
Reply

1,242 Views
zhuyuechong1
Contributor I

We check the CTE clock frequency ,the frequency is "0"

We do not know what is wrong with the CTE clock configration.

{.clockName = CTE0_CLK,

.mc_me_RunPeriphConfig = MC_ME_PERIPH_CONFIG_1,

.mc_me_LowPowerPeriphConfig = MC_ME_PERIPH_CONFIG_0}

Tags (1)
0 Kudos
Reply

1,323 Views
zhuyuechong1
Contributor I

other register can be read and write ,such as SIUL2 register:"SIUL2.MSCR[43].B.src=3"

0 Kudos
Reply