Possibility of using lin master node to receive lin frames from other master nodes(MPC%/$(G)

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Possibility of using lin master node to receive lin frames from other master nodes(MPC%/$(G)

659 次查看
ZD-Zhengkun
Contributor II

Hi,

I am using MPC5748g to receive lin frames, but according to the reference manual, only LINFlexD0 can be configured as the slave node, the others can only be configured as lin master. Thus, I have a question, is it possible to use LINFlexD1~17 as the master node and receive the lin frames from the other master nodes? Since they can receive the frames from slave nodes that contain only data without a header, is there a solution to extract the data from frames(wither header) from other master nodes?

BR,

Zhengkun Li

标记 (3)
0 项奖励
回复
1 回复

650 次查看
davidtosenovjan
NXP TechSupport
NXP TechSupport

I am not completely sure if i understand what you want to achieve. Do you want to perform the test as shown in the following example code?

https://community.nxp.com/t5/MPC5xxx-Knowledge-Base/Example-MPC5748G-LINFlex-LIN-Master-Slave-test-G...

 

 

0 项奖励
回复