Need AUTOSAR TCP/IP stack without FreeRTOS on MPC5777C

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Need AUTOSAR TCP/IP stack without FreeRTOS on MPC5777C

5,961 Views
ajmerijaimin
Contributor III

Hello NXP,

I am working on MPC5777C microcontroller. We have used EB Tresos tool to configure the ethernet driver.

We are looking for Classic AUTOSAR compliant TCP/IP stack without FreeRTOS for implementing the bootloader that uses the Ethernet interface.

Please suggest the best way without RTOS.

Regards,
Ajmeri Jaimin

0 Kudos
Reply
4 Replies

5,942 Views
cuongnguyenphu
NXP Employee
NXP Employee

Hi,
If you don't want to use RTOS, then Bare-metal embedded system approach is a choice.
Setup your Stack inside a task within a super loop :

 



0 Kudos
Reply

5,936 Views
ajmerijaimin
Contributor III

Hi @cuongnguyenphu ,

I now have this perception of the super loop. I will check further to understand how to compile it. I have a question. Is the stack AUTOSAR compliant? can you please confirm?

0 Kudos
Reply

5,900 Views
cuongnguyenphu
NXP Employee
NXP Employee

It depends on how you implemented in that super loop. NXP package for MPC only focus on Autosar MCAL layer, while TCP/IP stack is placed between Socket Adaptor and EthIf layer.

cuongnguyenphu_0-1664179173851.png

Can you refer these topics below for some solution of FNET and LwIP to use TCP/IP stack. But I'm not sure about the Autosar compliant of these solutions:|
https://community.nxp.com/t5/MPC5xxx/does-anybody-have-a-TCPIP-library-compiled-for-MPC5775k-or/m-p/...

https://community.nxp.com/t5/S32K/AUTOSAR-TCP-IP-stack/m-p/925261

 

0 Kudos
Reply

5,795 Views
ajmerijaimin
Contributor III

Just an update.

I've ported LWIP for our project and I've used it NO_SYS for bare-metal. It's working fine with MCAL drivers.

We are aware that LWIP is not AUTOSAR compliant. I think it's best to keep AUTOSAR compliant aside and continue to work on the remaining stuff. Because I belive the stack can be swapped later.

Thanks for the support.

0 Kudos
Reply