NXP MPC5744P CAN Bootloader

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

NXP MPC5744P CAN Bootloader

1,317 次查看
C_Zuercher_APR
Contributor III

Hi,

I'm looking at using a Bootloader which can flash my ECU via the CAN Bus with an array of USB/CAN Dongles (not just Vector Hardware).

In addition, I'd also like to be able to flash the ECU via a 3rd party GUI which I would write.

Are there any recommendations for any NXP/3rd party bootloaders?

Thanks,

Crispin

标记 (2)
0 项奖励
回复
1 回复

1,309 次查看
lukaszadrapa
NXP TechSupport
NXP TechSupport

Hi Crispin,

We have this application note which can be used as a starting point to develop own solution:

https://www.nxp.com/docs/en/application-note/AN5319.pdf

https://www.nxp.com/docs/en/application-note-software/AN5319SW.zip

If we are talking about 3rd party bootloaders, I can remember this one:

https://www.vector.com/int/en/products/products-a-z/embedded-components/flash-bootloader/

Regards,

Lukas