MPC5775B IEC 60730 Class B library

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

MPC5775B IEC 60730 Class B library

2,042 次查看
MarkFan
Contributor III

Hi everyone.

Does NXP have a "IEC60730 class B safety library" for MPC5775B?

or any good advice to pass the IEC 60730-1 class B test.

Thanks for any help.

 

Mark

0 项奖励
回复
6 回复数

2,030 次查看
MarkFan
Contributor III

Hi Peter,

    Thanks for your rapid and clearly reply. Actually, this is a BMS for ESS solution.

    As you said the automotive standards are more strict, however we need to prove it. 

   How can I get the Safety application Framework? 

Best regards,

Mark

    

0 项奖励
回复

2,021 次查看
petervlna
NXP TechSupport
NXP TechSupport

Hello,

Hmm, looking at SAF (framework) it supports only S32 devices.

petervlna_0-1664434972519.png

So it is not suitable for MPC5775B which is previous architecture family.

Then only thing available is safety application guide. By following suggested countermeasures you can reach ASIL-D.

Such guide is located at safe assurance community:

petervlna_1-1664435090039.png

https://community.nxp.com/t5/SafeAssure-NDA-group/MCUs-MPUs-available-Functional-Safety-documents-Sa...

there is restricted access and you need to follow attached document in order to get access.

Best regards,

Peter

0 项奖励
回复

2,038 次查看
petervlna
NXP TechSupport
NXP TechSupport

Hello,

You are asking about automotive micro, the standard it can reach is ISO26262 ASIL-D.

No home appliance libraries for industrial use case are available for automotive micro.

https://www.nxp.com/products/product-information/product-programs/iec-60730-safety-standard-for-hous...

But since automotive standards are more strict you can probably use Safety application Framework (part of AUTOSAR) to reach your requirements.

Not sure why you would use such safety and security micro with automotive peripherals for home usage. Not talking about auto chip shortage. That would be just overkill.

Best regards,

Peter

0 项奖励
回复

2,004 次查看
leonggz
Contributor I

hello, to follow this thread, is there a "safetylib" for the MPC5777C/75E/75B ? i did download the mpc5777C mcal autosar from the nxp official website but i don't see any mention of the safety application framework term.. please shed a light.. thank you.

0 项奖励
回复

1,912 次查看
MarkFan
Contributor III

Hi,

    As Peter said the automotive standards are more strict, however we just need to prove it, Maybe we can help each other or someone else has passed the test could give us a hint. below are the solution I have check with safety application guide for now.

| Component | Solution 
| 1.1 Register |  BIST 
| 1.3 Programme counter | Test Function |
| 2. Interrupt handling execution | Test Function | 
| 3. Clock | CMU 
| 4. Memory |
| 4.1 Invariable memory |BIST
| 4.2 Variable memory | BIST 
| 4.3 Addressing | BIST | 
| 5. Internal data path | 
| 5.1 data |  ERM | 
| 5.2 Addressing | ERM |
| 6. External communication | CAN
| 6.3 Timing | Test Function
| 7. Input/output periphery | Test Function 
| 7.2 Analog I/O | no used | 
| 7.2.1 A/D- and D/A-convertor | Test Function | 
| 7.2.2 Analog Multiplexer | no used 
| 9. Custom Chips for example : ASIC, GAL, Gate array | no used 

I only implement BIST online function for now. Plan to implement other test function or  Safety Mechanism.

question  :

1. How to get the PC counter?

2. Interrupt handle for ERM?

Thanks for any help or suggestion.

Best regards,

Mark

  

 

0 项奖励
回复

1,993 次查看
petervlna
NXP TechSupport
NXP TechSupport

Hello,

As I have posted earlier the SAF is not supporting SPC5775E/B device.

Best regards,

Peter

0 项奖励
回复