Hello,
according to "Document Number: MPC5746CRM Rev. 4, 12/2016" the Calypso 3M derivatives no longer support the FMT1 Format for the System MPU. (Appendix A: Release Notes, General Changes "Removed "Region Descriptor n, Word 2 Format 1 (SMPU_RD_nW2_F1)" register" - page 3396).
Is this information correct for all Calypso3M derivatives ? Is there a mask set which supports FMT 1 ?
What about Calypso6M ? Will there be changes too ?
I need to ask because for our AUTOSAR OS we need to distinguish between Supervisor- and User Mode on memory access control. But from our point of view this isn't possible with this derivative if only FMT 0 is supported. Is this correct ?
Thanks in advance and best regards
Martin Schultheiß
解決済! 解決策の投稿を見る。
Hi,
I finally got an answer:
The changes to the RM with respect to FMT = 1 not now being supported are NOT correct. FMT =1 IS supported by both Cal 3M and Cal6M. There is an update to the reference manuals about to be released to reflect this.
Peter
Hi,
I finally got an answer:
The changes to the RM with respect to FMT = 1 not now being supported are NOT correct. FMT =1 IS supported by both Cal 3M and Cal6M. There is an update to the reference manuals about to be released to reflect this.
Peter
Hi Peter,
thank u for the information. I'm glad to hear that.
BR
Martin
Hello Martin,
I have asked doc and apps team for clarification.
I will feedback you ASAP.
Peter