MPC5604 support CAN3

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MPC5604 support CAN3

504 Views
玉利崔
Contributor II

 i want  to know whether MPC5604 is support CAN3,the  MPC5604B/C Microcontroller Data Sheet write that CAN0, CAN3 and either CAN1 or CAN4 are available. CAN2, CAN5 and CAN6 are not available,but the  MPC5604B/C Microcontroller Reference Manual write that CAN0, CAN1 and CAN2 are available. CAN3, CAN4 and CAN5 are not available.

0 Kudos
Reply
1 Reply

433 Views
PetrS
NXP TechSupport
NXP TechSupport

Hi,

as far as I know the RM's footnote 7 is wrong, the correct is the one from DS; CAN0, CAN3 and either CAN1 or CAN4 are available. CAN2, CAN5 and CAN6 are not available.

So except of 64pin MPC5604B, the CAN3 is available.

BR, Petr

0 Kudos
Reply