MCU SPC5744PFK1A & S9KEAZ128AMLJ MTTFd Values

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MCU SPC5744PFK1A & S9KEAZ128AMLJ MTTFd Values

1,187件の閲覧回数
Louis1916
Contributor II

The products require certification,need SPC5744PFK1A & S9KEAZ128AMLJ MTTFd Values, How can I request relevant documents(FIT),Thanks!

0 件の賞賛
返信
4 返答(返信)

1,147件の閲覧回数
petervlna
NXP TechSupport
NXP TechSupport

Hello,

Here are FIT for SPC5744P.

For Kea device, please ask at the S9KEA forum.

Best regards,

Peter

0 件の賞賛
返信

1,137件の閲覧回数
Louis1916
Contributor II
Hi Peter
Thanks very much!
0 件の賞賛
返信

1,176件の閲覧回数
prakashram72
Contributor III

Hi @Louis1916,

For the SPC5744PFK1A and S9KEAZ128AMLJ, you can find the MTTFd (Mean Time To Dangerous Failure) values in the respective product's datasheet or reliability report. These documents provide detailed information about the product's reliability, including the MTTFd values.

For the SPC5744PFK1A, you can find the datasheet here. The reliability report can be found here.

For the S9KEAZ128AMLJ, you can find the datasheet here. The reliability report can be found here.

If you need the FIT (Failure In Time) rates, these are typically provided in the reliability report. If you cannot find the information you need in these documents, you may need to request additional documentation from NXP.

Please note that the actual MTTFd and FIT values can depend on various factors such as the operating conditions and the specific application of the product. Therefore, the values provided in the datasheets and reliability reports should be used as a guideline, and the actual values may need to be calculated based on your specific use case.

1,136件の閲覧回数
Louis1916
Contributor II
Hi Praka
I don't have permission to access on this server ,So can you send it of adding an attachment about S9KEAZ128AMLJ,Thanks!
0 件の賞賛
返信