How to add leds to indicate the state of FCCU0 and FCCU1

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How to add leds to indicate the state of FCCU0 and FCCU1

886件の閲覧回数
AllanAn
NXP Employee
NXP Employee

PL see the picture below:

FCCU.PNG

what's the state of FCCU0 and FCCU1  ("0" or "1"),  when an error occurs ?

I want to add leds to indicate the state of FCCU0 and FCCU1, where can I add them?

if FCCU0 and FCCU1 have the ability to drive the LED(about 2mA) ?

Thank you for your answer !

0 件の賞賛
返信
2 返答(返信)

725件の閲覧回数
davidtosenovjan
NXP TechSupport
NXP TechSupport

Hi, if you use bi-stable protocol, then you could possibly use these signal for driving LEDs.

pastedImage_1.png

I would recommend to drive base of the transistor and put LED to the collector of the transistor. Of course, some resistors will be needed to use to set right working point.

Here I have found some article for inspiration:

Driving an LED using a Transistor 

Hope it helps

0 件の賞賛
返信

725件の閲覧回数
AllanAn
NXP Employee
NXP Employee

OK, thank you very much, David

BRs

0 件の賞賛
返信