How can i make MK20 works as on board OpenSDA debugger tool.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How can i make MK20 works as on board OpenSDA debugger tool.

1,128 Views
haoxue1027
Contributor V

hi,

Now I have one new  MK20DX128VFM5 . 

I want to make it works as on board OpenSDA debugger tool with the MPC5744P .

Is the  MK20DX128VFM5 need for debuging .

how to do it .

OpenSDA Serial and Debug Adapter | NXP where provide the methods to update your board with OpenSDA applications. however , I can not find the MPC5744P type of the option.

pastedImage_3.png

Can you help me to find the methods .

best regards

hao

0 Kudos
Reply
4 Replies

1,008 Views
Sabina_Bruce
NXP Employee
NXP Employee

Hello,

Our website provides the binary downloads for the freedome development or tower boards. I recommend that you download the generic OpenSDA firmware, which you can find on the segger website. As shown below:

pastedImage_1.png

If you would like to test the functionality before creating your custom board, I would recommend to use another evaluation board that we offer and download the generic firmware on to it so you can begin your testing.Also, the boards that have been tested and confirmed to work are on the following site. Please keep in mind that it is not guaranteed to work with the MPC5744, if you have any doubts regarding the firmware you can also contact segger.

Best Regards,

Sabina

0 Kudos
Reply

1,008 Views
haoxue1027
Contributor V

Hello,

thanks for replying.

The website say that generic OpenSDA firmware supports all ARM based NXP

but DEVKIT-MPC5744P evaluation board  is Power Architecture.  is it  not sure to support PA?

 best regards

hao

0 Kudos
Reply

1,008 Views
Sabina_Bruce
NXP Employee
NXP Employee

Hello,

That is correct the OpenSDA is tested to function with ARM based devices. However the development kit we provide for the MPC5744 also uses OpenSDA, unfortunately we do not provide the source file for the one used in this kit. 

This is why I recommend to previously attempt with another microcontroller if you have one available with the generic OpenSDA firmware. 

It is not guaranteed to work.

The other option you have instead of using OpenSDA, is to work with external debugger tools.

Best Regards,

Sabina

0 Kudos
Reply

1,008 Views
haoxue1027
Contributor V

Hello

thank for replying.

Now, it is not guaranteed to use OpenSDA for MPC5744.

it is still not available to debugger based on MBD.

How to export Generated Code to S32 Design Studio IDE (applicable for MBDT for MPC5744P v2.0)  

In this situation, the development board is really too difficult to use it.

 best regards

hao

0 Kudos
Reply